Part Number: TPS56221 Hi TI team
for the thermal test of the TPS56221EVM , What are the test conditions (ambient temperature ,test time) to reach a maximum temperature 86°c like the datasheet ?
...
and thanks .
Part Number: TPS56221EVM-579 Other Parts Discussed in Thread: TPS56221 Hi ti team
i want to know what's The conditions of this experimental tests of TPS56221 eval bord
(was the card oriented vertically or horizontally? the card was on a wooden or plastic…
Part Number: TPS56221 Hi team,
Could you give the min and max value of the package height for TPS56221?
Need this information in order to attach a heatsink.
Regards,
Noriyuki Takahashi
Part Number: TPS56221 Is there a way to disable compensation loop/components on this controller? Due to large variation in filter components used there is no way to match compensation loop perfect (and rarely happens in real life since many ceramics do…
Part Number: TPS56221 Hi,
Can you help advise on two strange operations? I don't think it's a stability issue. Do you think it would appear in bench as well? How do I improve it?
(1) overshoot and dip during the startup
(2) VOUT voltage dc…
Part Number: TPS56221 Hello Team,
Is there a test data of output current vs. Tj/Tc? There's a similar figure in datasheet but it's measured by Ta.
Thank you!
Part Number: TPS56221 Hi,
Is it possible to measure the resistance between Vout and GND without power on TPS56221 EVM?
My customer finished to assemble the board. Before supplying input_power, he measured resistance between Vout and GND to confirm correct…
Part Number: TPS56221 Other Parts Discussed in Thread: TPS53353 , , TPS543B20 , TPS53355 Hello, My customer would like to design Vin=12V, Vout=5V and Iout(max)=16A buck convertor at Ta=85oC. They are considering either TPS56221 or TPS53353, take a look…
Part Number: TPS56221 Other Parts Discussed in Thread: TPS56121 , Hi team
Could you help check if we have P2P alternative of TPS56221 in addition to TPS56121? Thank you.
Part Number: TPS56221 I am using TPS56221DQPT under the following conditions:
Vin = 12 Vout = 0.85 Fsw = 1 MHz Target Imax = 15 A Target Ipp = 5.2 A
With no load the regulator hits the target voltage. However as soon as I give it more than ~500mA load, the…