Part Number: TPS563249 I would like to know the rated power when connecting a resistor to the VBST terminal.
Please tell me the input impedance of the VBST terminal.
Part Number: TPS563249 Other Parts Discussed in Thread: TPS563201 , TPS56339 Hi,
My customer is using TPS563249 for generating a 5V output rail from a 12V input. The maximum output current required is 2A. But the Supply of TPS563249DDCR is highly constrained…
Part Number: TPS563249 Other Parts Discussed in Thread: TPS62913 We found issue in one of our field returned device. Our Front end module of WIFI IC is getting damaged at it's power pins.
We can replicate this issue by providing 6V to our Front end…
Part Number: TPS563249 Hello,
I would appreciate any feedback to the questions below regarding DCDC converter TPS563249.
Currently the device (TPS563249) is not performing thermally at the specification it needs to perform at.
Is it possible to lower…
Part Number: TPS563249 Order number: T01147185
MPN: TPS563249DDCR
Issue: DUT stop function in a sudden, and find out TPS563249DDCR output short to GND
observation:
- TPS563249DDCR Input, Output, and GND pins all short together.
- resistance between these 3…
Part Number: TPS563249 Other Parts Discussed in Thread: TPS56339 Hello Guys,
Good day.
Based on Table 2 "Recommended Component Values" of the datasheet, the maximum output voltage for TPS563249 is up to 6.5V only. Is this the maximum or its possible to…
Part Number: TPS563249 Other Parts Discussed in Thread: TINA-TI , , PSPICE-FOR-TI Hello,
The TPS563249DDC SPICE model that is available on TI.com is encrypted and will not correctly import into TINA-TI.
Is there an easy way to decrypt this file?
Part Number: TPS563249 Other Parts Discussed in Thread: TPS56339 Tool/software: WEBENCH® Design Tools Hi,
I would like to use web bench to design a voltage regulator circuit with TPS563249. My input voltage is DC 12V and output is DC 5V, current is 3A…