Part Number: TPS565201 Other Parts Discussed in Thread: AMC1200 , , TPS561208
Hello ,
I am using AMC1200SDUBR as an isolation amplifier in a voltage measurement PCB. I have a large quantity of the boards and they are behaving in a similar manner.
In order…
Hi Fan-san,
I request to fix the TPS565201 _TRANS PSpice model of the "TPS565201 Unencrypted PSpice Transient Model Package (Rev. A)".
You ran the transient simulation of TPS561201 .
Best Regards,
Koshi Ninomiya
Part Number: TPS565201 Dear team
The customer would like to know, which value of the current limit (IOCL)?(RMS value or peak value)
Refer from datasheet page.5.
Many thanks
Denny
Part Number: TPS565201 Dear team
The customer would like to add second source RT6264 to avoid material shortage. They need add R54(10Kohm) in the circuit.
Will R54 affect the TPS565201DDCR?
Many thanks
Denny
Part Number: TPS565201 Dear team
The customer
1. Whether the resistance value of R6579 and R6576 has a limited range, otherwise it will cause insufficient current driving ability.
2. Whether to consider REN in the calculation, the equivalent circuit…
Part Number: TPS565201 Hi team,
According to the datasheet, min off time is specified at max 280ns and Fsw is typ 500kHz.
For 5V output requirements, Vin would need more than 6V with the above conditions
Is that correct ?
Thank you and best regards…
Part Number: TPS565201 Other Parts Discussed in Thread: TINA-TI Hi,
I'm using the TPS565201 and need to have a total of 150uF of Cout (15 x 10uF MLCC). My output voltage is 5V and I'm using L=10uH. The datasheet says max Cout is 68uF. I have seen…