Part Number: TPS61021EVM-723
Hi Experts,
Our customer would like to request if he c ould have a copy of the design files for this module. He is using Altium which is what he believe our designs are designed with.
Best regards, Gerald
Part Number: TPS61021EVM-723 Other Parts Discussed in Thread: TPS61021A Hi,
I am using Re-chargeable Nimh AA battery (1.2v) at Input of "TPS61021EVM-723" Board and "5.5ohm" fixed load is connected to the output of Board to pull fixed current (approximately…
Part Number: TPS61021EVM-723 I'm testing the output current of the TPS61021EVM (Vout = 3.3V) with different load resistors and am not getting results comparable to the datasheet.
When Vin = 1V, the maximum Iout is ~150mA (RLoad = 22 Ohms).
With an…
Part Number: TPS61021EVM-723 Hi everyone,
I'm currently working on a design with this chip. The input is 3.3V and the output is typically 50mA (current driven in MCU). SuperCap is also plugged in the input so when the power is shut down it survives for…
Part Number: TPS61021A Other Parts Discussed in Thread: TPS61021EVM-723 , Hi,
What is the typical and maximum shutdown current into the VOUT pin (EN low, Vin 3.0V, Vout 3.3V, Tj -40, +25 and +85°C)?
Regards CHA
Part Number: TPS61021A Other Parts Discussed in Thread: TPS61021EVM-723 Hi,
I am evaluating the TPS61021A device by obtaining the evaluation board. The evaluation board is TPS61021EVM-723. So I have some questions about how to use the device. · What is the…
Part Number: TPS61021A Other Parts Discussed in Thread: TPS61021EVM-723 , Hi
I use the TPS61021EVM-723 to test a new DC-DC desing powered by a 1.5V battery. I use Webench to start the design. The lower startup input voltage is state to be 0.9V by Webench…