Part Number: TPS61041-Q1 Hi Team,
My customer has been using TPS61041AQDBVRQ1 before and now as stated in the datasheet, this deice is in LIFEBUY status so customer wants to use TP61041QDBVRQ1 instead.
Could you please specify the difference of those…
Part Number: TPS61041-Q1 Hello TI-teams,
I designs dark current and comsumption current for TPS61041-Q1,but we do not have enough information for calculation from datasheet .
So, Could I ask any questions for quiscent current?
Question 1.
I understand…
Part Number: TPS61041-Q1 Hello, I am working on a boost converter circuit simulation on PSpice using the TPS61041-Q1 to try and boost 5V to 10V, however it is not functioning properly and it is only outputting 5V. I would like some help in determining…
Part Number: TPS61041
Hello Team,
When my customer doing Vout short test, TPS61041 goes burned.
I guess it is because the high current goes into IC when Vout is shorted. So, I was looking for Over Current Protection of TPS61041, but it is hard to find…
Part Number: TPS61041 Hello,
For this device, how is the output voltage rise time affected by inrush current? For example, if I have a load switch limiting the inrush current to 150mA, how much variance could I see in the rise time of Vout?
Thanks, …
Part Number: TPS61041-Q1 Hi team,
Can we share what the difference is between the devices?
Both are online and available for customers to purchase, but I can't find a clear differentiation.
Thanks,
Jacob
Part Number: TPS61041-Q1 Other Parts Discussed in Thread: TPS61041 Hi team,
We find there is A version for TPS61041-Q1 in system but we can't find further information for customer.
So please help to provide comparison table for study.
Thanks
TPS6…
Part Number: TPS61041-Q1 Other Parts Discussed in Thread: TPS61041TPS61041-Q1 has load current rating of 250mA, I need to design a circuit with load current 120mA, but with the calculation which was mentioned in
Datasheet, I'm not able to meet 120mA…
Part Number: TPS61096A Other Parts Discussed in Thread: TPS61041 , Hi Expert,
This is Koki Tsushima.
My customer will evaluate EVM of TPS61096A, but wants to know why this efficiency lower than TPS61041 at Vout 12V, Iout 1mA ?
As fig.1 that efficiency…
Part Number: TPS61041 Hi,
I am inspecting TPS61041QDBVRQ1 which shows a top marking that I have not seen before. (red arrows)
Usually TEXAS top marking are in dashes, however, this part is in blocks.
I have attached pictures to show the difference (circled…