Part Number: TPS61046 Other Parts Discussed in Thread: TPS61096A Hi team,
Could you help check if we get the following boost part recommendation?
Number of Output
VIN
VOUT
IQ
ILoad
1
2V ~ 3V
8V
28uA Max.
5mA Max.
Thanks and…
Part Number: TPS61046 Hi,
I am writing to request your assistance in improving the efficiency of a boost converter circuit in our design.
We are currently using the TI TPS61046YFFR to convert a LiPo battery voltage (3.0V to 4.35V) to 10V for powering…
Part Number: TPS61046 Hello, I want to calculate the switching losses for the internal MOSFET. I could not find the turn on, turn off time & gate charge for the FETs in the datasheet. Please can you help to share these.
Part Number: TPS61046
Dear FAE
My project requirement is to get different voltage levels (Vout=5V-20V) from the booter (with Vin=3.3V) based on other input conditions, I plan to do it by a resister network of R1.
Take Figure 11 from the datasheet, I…
Part Number: TPS61046 Dear Friend
I can't find an indicator of pin A1 for this BGA package (TPS61046YFFR), I am wondering if there is one.
If yes, maybe my magnifier is not good enough, if not, please let me know.
Thank you
Tony
Part Number: TPS61046 Hello, The app note SLVA372D – REVISED NOVEMBER 2022 (attached below) mentions that for a CCM Boost design the Inductor Current to be 20% to 40% of Output current. I think it should be the % of Input DC Average current. Please can…
Part Number: TPS61046 Other Parts Discussed in Thread: TPS61372 , TPS61086 Hi Team,
Can you help to check if we have any devices spec similar to TPS61046, but with Force PWM mode only to reduce output ripple? Thanks.
Part Number: TPS61046 Hi team!
I dis the simulation of TPS61046. But there is no output waveform. And the window jumped as below. Whatever I clicked, there is no change and no waveform. Can you help solve this issue?
Part Number: TPS61046 Other Parts Discussed in Thread: TLV61046A , TPS61040 Hi team,
I'd like to find a boost device that can support below conditions. I can see TPS61046 is suitable and I just want to check if there is another suitable device.
Vin…
Part Number: TPS61046 Hi team,
My customer was wondering more about this over-voltage protection feature.
If the output voltage exceeds the 28V condition, does this mean the output is effectively disconnected from the load? Does it produce any output…