Hi Zack,
I sent the schematic with private message.
Could you please confirm and advise by Aug 3rd.
I appreciate your great help and cooperation.
Best regards,
Shinichi
Part Number: TPS61086 Other Parts Discussed in Thread: LM5157 Dear Specialists,
My customer'd like to know Postive(+15V) and Negative(-15V) Voltage Power Supply Design with the coupled SEPIC and Inverting SEPIC by TPS61086.
Vin 5V, Vout +15V/-15V 100mA…
Part Number: TPS61086 Hi team,
My customer is intend to add snuber circuit between SW and GND to reduce a noise on TPS61086. Could you tell me the recommended initial value of the Rsnub and Csnub?
Vin=3.3V, vout=3.9V, Iout=0.6A(max), Mode=High.
regards…
Part Number: TPS61086 Hi team,
My customer is evaluating the TPS61086EVM.
The customer is measuring the frequency response, but they cannot get enough phase margin of the TPS61086. (Iout = about 0.3A, which is about 30deg).
They tried following comp values…
Part Number: TPS61086 Other Parts Discussed in Thread: TPS61089 , TPS61175 , LMR62014 Hi team,
My customer would like to use the TPS61086 for the following condition.
Vin=5-9V
Vout=9V
Iout=600mA
Does TPS61086 allow to separate input rail as shown below…
Part Number: TPS61086 Hi Team,
Just want to check with you why Vout min is Vin+0.5V. what's the limitation on the mini Vout, is it duty cycle or others? Thanks.
BRs
Given
Part Number: TPS61086 Hi TI Experts,
I plan to use TPS61086.
Input Voltage: 3.0 to 4.2V (Supply from a Rechargeable Lithium Polymer battery)
Output Voltage: 6V
Current consumption: 500 ~ 550mA
At the datasheet, the Output Voltage is Vin+0.5V to 18.5V…
Part Number: TPS61086 Hi team,
Fig. 22 in the datasheet shows the over voltage protection circuit by a zener diode and Rlimit.
Could you explain me how to choose the breakown voltage of the zener diode and Rlimit value?
Regards,
Saito
Part Number: TPS61086 Hi team,
I'm curious about the reason why there is a limitaion that Vout should 0.5V higher than Vin.
Is it caused by the minimum PWM pulse width limitation in the IC?
Regards,
Saito