Part Number: TPS61096A Hi,
I have two questions related to level shifters.
1. When device is disabled (EN=0V) and LVIx is logic high, what would be level on HVOx?
2. Electrical specs on page 5 list level shifter sourcing and sinking current to be…
Part Number: TPS61096A I found this app note: https://www.ti.com/lit/an/slvaf38/slvaf38.pdf
Do we have Altium files for this board sitting around somewhere...?
Regards,
Darren
Part Number: TPS61096A Hi expert,
This is Koki Tsushima.
My customer wants to know the proper inductance value.
Q.1
What is the meaning of the minimal of the last sentence? - Is it the recommended min, which is 1uH?
Q.2
Is this calc…
Part Number: TPS61096A Other Parts Discussed in Thread: TPS61041 , Hi Expert,
This is Koki Tsushima.
My customer will evaluate EVM of TPS61096A, but wants to know why this efficiency lower than TPS61041 at Vout 12V, Iout 1mA ?
As fig.1 that…
Part Number: TPS61096A Dears currently used TPS61096A for variable output application through switching dedicated resister divider using external - mosfet ,
so couly you help check below parameter may related with my application
1. Vosns - output…
Part Number: TPS61096A Hi Expert,
This is Koki Tsushima.
My customer evaluates EVM now but for EVM, GRM188R6YA106MA73D*2pcs are adopted for Cout.
My customer wants to use maximum highest Vout, which is 28V, but for that time, GRM188R6YA106MA73D…
Part Number: TPS61096A Other Parts Discussed in Thread: TLV61046A HI TI expert,
I have the requirements as below:
Vin=2.5~3.3V
Vout=12V
Iout max=80mA
TPS61096A is selected for our design to meet the above requirements.
But when I try to generate…
Part Number: TPS61096A
Hi experts,
This is Koki Tsushima,
Customer wants to know efficiency curve when 5V output like this.
Is it possible to share with me?
I guess customer wants to use this by 1LiPo so Vin =3~4.5V.
Iout is few mA~ up…
Part Number: TPS61096A Hello,
What is the functionality of VOSNS pin in TPS61096A boost converter. Is it for remote sensing for taking the feedback from load?
Please explain what it is and what are its functionalities / advantages? Thanks in advance…