Part Number: TPS61098 Hello team,
I am wondering what is the current limit in the VBUS output pin in TPS610981 and TPS610986 chipset??? I denoted that load switch on resistance in TPS610985/6 are 1.2Ohm (typical) and LDO dropout voltage in TPS61098/1/2/7…
Part Number: TPS61098 I have 3V as input and i need 3.3V as output using " TPS61098" i tried in real life it only pass the input to the output and no boosting action.
Can somebody help?
I was planning to buy "TPS610986" but there were no stock…
Part Number: TPS61098 Hello Expert,
I have some questions.
1. Is the difference between ACTIVE MODE and LOW POWER MODE just the difference of turning off the internal LDO/load switch (Vsub) and keep on boost?
2. Is there any difference between MAX output…
Part Number: TPS61098 Other Parts Discussed in Thread: TPS63802 ,
I'm trying to build a project where the source voltage is a standard 18650 battery. But the circuit requires 2 voltages - 3.3 and 1.3. 3.3V is for digital (MSP430) and analog (audio…
Part Number: TPS61098 Hello Experts, My customer would like to know the efficiency variation via temperature. Could you provide it? The efficiency is usually decreased at high temperature due to RDSon will be increased. Is my understanding correct? Best…
Part Number: TPS61098 Hi
I have a question about TPS610985. If I used MODE terminal as being fixed low and I doesn't use Vsub, should I use capacitor between Vsub and GND?
Best regards,
Yokota
Part Number: TPS61098 Dear TI experts,
We are designing a voltage booster using TPS610985 for smart lock application. The system needs to boost input voltage from 2V to 3V output and deliver 100mA current. We put together the design based on the reference…
Part Number: TPS61098 Other Parts Discussed in Thread: TPS61089 Hi,
I am using TPS61098 to boost voltage from LiFePo4 battery (3.2V to 2.9V) to 6 volts to drive this motor: Thomas G6/02-8
The motor draws 0.5A - 1A of current
My schematics are below, the…