Part Number: TPS61099 I'm considering 3.0V fixed type of TPS61993. I've selected the inductor to LQM18PN1R0MFHD. If there is concern or problem, Could you advice to me? My product's setting is below.
Input voltage :0.7~1.5V Output Voltage :3.…
Part Number: TPS61099 Hello,
I'm designing a board with TPS610995, Vin between 0.8 and 1.4V. The EN pin will be controlled by a MCU powered by a 3.0V ULP pumpcharge regulator. Is it ok for TPS61099x to have a EN voltage (3.0V) greater than VIN voltage…
Part Number: TPS61099 Hi team,
Could you please let me know about the Iq definition of TPS61099?
The condition is specified as "IC enabled, no Load, no Switching".
I wonder that because as long as the IC is enabled, the IC must be switching even…
Part Number: TPS61099 Other Parts Discussed in Thread: TPS61094 , TPS61021A , TPS61023 Hello, I search a boost convertor at TI.com based on the following requirements. Vin= 3.3V Vout=3.9V Iout(max)=0.5V Then TI.com showed total 89 devices. I selected TPS61099…
Part Number: TPS61099 I have a LiPo battery cell with a voltage from 2.7V to 4.3V roughly. I would like to use this power source as the input of the TPS61099 3.3V fixed output. Is it alright that the input is greater in voltage than the output?
Part Number: TIDA-01580 Other Parts Discussed in Thread: TPS61099 , TPS61099 is outputting 4.2V for Tx_SUP. Why 4.2V is selected for TX supply when it can accept anything between 3-5 V?
Part Number: TPS61099 Hi,
I'm planning to use TPS61099DRVR part in my product.
I have a question that can this boost converter works reliably when input voltage reaches close to output voltage set by feedback resistors.
So my input can be from…
Part Number: TPS61099 I would like to have my TPS610996 schematic design reviewed if possible. Please let me know who I should send it to or if I should just post it.
Part Number: TPS61099 Hi Team,
My customer is using TPS610994 boost from +2.8V to +3.3V with load around 30~70uA output, however customer got +5.xV output voltage sometimes.
the output voltage can back to normal +3.3V output if customer short the output…
Part Number: TPS61099 I am considering using tps610996 in a new design and would like to use webench to help select specific components. Currently tps610996 does not come up as an option in webench even though the other fixed voltage versions do. Is there…