Part Number: TPS61099 Other Parts Discussed in Thread: TPS61299 Duck 3 C.pdf
Recently our customers are using this material. When the customer uses, the measured light load efficiency is 40%, but spec is 75%, please help to see if there is a problem…
Part Number: TPS61099
Tool/software:
Hi team,
When this device is operated below condition. It is observed that the current consumption increase up to about 10mA in a cycle of about 20 ms.
・Using EVM circuit ・Vin=1.5V ・Vout=3.1V ・No load
I guess…
Part Number: TPS61099 Tool/software: Hi,
The MSL level of part SN1807032DRVR in the datasheet is Level-1, while in my received part's label is Level-2. Is it normal?
Part Number: TPS61099 Dear Sir,
Please refer to following waveforms shown in TPS61099 datasheet. According to input/output voltage conditions, duty cycle should be 0.5747, but what waveform shown doesn't match. Why?
Best regards,
Genie
Part Number: TPS61099 Tool/software: Dear Sirs!
I am going to use TPS61099YFF in following conditions:
Vin 1.05-1.65V
Vout 3.3V
Question. Can enable input be connected to port of controller? Voltage is 1.8 V. It is higher then Vin. Can it cause…
Part Number: TPS61099 Other Parts Discussed in Thread: TPS61299 , , TPS610985 , TPS61299A
Tool/software:
Hi TI team,
We are designing an application with the following design configuration.
Basically, the design includes 2x batteries Li…
Part Number: TPS61099 Other Parts Discussed in Thread: TPS61299 Hi TI Teams,
One of our customer reported that the efficiency is only 74%~76% with the real load like MCU,small fan and laser (the laser is switched on at 0.5s intervals, and the other…
Part Number: TPS61099 Hi Team,
ON BGA layout.
It says to do this layout where the GND is VIA’d to a large GND plane on bottom side. Understood.
I do have large GND on bottom side, but I also have top side flooded with GND.
Can I let the GND…
Part Number: TPS61099 Other Parts Discussed in Thread: TPS61033 Is there a Boost Regulator with Integrated MOSFET having Pass-Through Mode for Vin range greater than 5.5V ? I see that Pass-through feature in Integrated MOSFET Boost are available for low…