Part Number: TPS61252 Other Parts Discussed in Thread: TPS61299 Dear TI
I'm Seunghyeon yun in charge of HW engineer.
We have plan for new portable device.
I would like your help in selecting parts.
Boost converter parts(ste up boost converter, buck…
Part Number: TPS61252 Hi team,
Do we have TPS61252 TINA file? The customer want to use this file to simulate frequency domain simulation? Or could you help simulate when Vin is 3.6V and Vout is 3.3V ,Io is 1.4A
Part Number: TPS61252 Other Parts Discussed in Thread: TPS63900 This is the first time I connect the circuit. I started using 3V6 and the VOut is the same as the VIn. When the VIn is below 3V3, the VOut remains at 3V3. The measurement was made with the…
Part Number: TPS61252 Hi,
This is the first time I connect the circuit. I started my tests using 3V6 and the VOut is the same as the VIn. When the VIn is below 3V3, the VOut remains at 3V3. The measurement was made with the processor without firmware…
Part Number: TPS61252 Hi, there was similar question some years ago, but with no clear answer. There is no data on PG max sink current. I do not need exact value, would just like to know if I can connect 100k resistor or 768K resistor instead of 1M, to…
Part Number: TPS61252 We’re going through a legacy design and see that the ILIM pin of TPS61252 is connected through a 0R resistor to ground. The datasheet recommends connecting the pin to Vin for maximum input current. What effect would grounding this…
Hi Ahmet,
Please kindly refer to below comments per your questions.
1. Can the capacitor used to absorb the energy be problematic in long run and if I put the tantalum capacitor near motor driver IC, will it also cause the loop stability issue you mentioned…
Part Number: TPS61252 Hello guys,
One of my customers is considering using TPS61252 for their new products.
They are worry about the case of FB terminal short to GND or open.
They have a few questions about the device as the follows.
Could you please…
Part Number: TPS61252 Other Parts Discussed in Thread: TPS61259 , TPS612592 , TPS61251 , TPS61253A Hi Power Folks,
Does TI have p2p device to TPS61252DSGR? Otherwise, could you also suggest any similar device even though it's not p2p? Thank you for your…
Part Number: TPS61252 Hi guys,
When the voltage of VIN and EN drops from 5V and gradually drops from 0.4V to around 0.3V (about 5 seconds), an event occurs in which VOUT rises from 0V to 0.3V. Is this the TPS61252 specification?