Part Number: TPS61280 Other Parts Discussed in Thread: , TPS61282D Hi,
I'm trying to use TPS61280 as a 2A,3.7V PSU for a microprocessor.
I'm not sure if my circuit is going to work based on the components I selected. I've created an analysis using…
Part Number: TPS61280 I use tps61280 for design. When debugging, I use DC power supply to input 3.6V voltage. After power on, it starts to output normal 4V. After about 1 minute, the output becomes 0. Vsel is connected to GND and en nbyp is high. The…
Part Number: TPS61280 Hi
What is the difference between TPS61280, TPS61280A, TPS61280D? What should I pay attention to when using it? What application is it suitable for?
Thanks
BRs
Elsa Duan
Part Number: TPS61280 Other Parts Discussed in Thread: TPS61256 , , TPS61282D , TPS61099 Hi,
We are currently evaluating a new material, a battery for silicon anode materials. This battery must be used with an IC with bypass function. Otherwise, the battery…
Part Number: TPS61280A Other Parts Discussed in Thread: TPS61280 , Hi Sir,
We plan to use TPS61280 part in our application. The part needs programmed by I2C for Boost threshold at 3V or 2.85V.
A socket board for DSBGA 16 package will be used for every…
Part Number: TPS61282 Other Parts Discussed in Thread: , TPS61280D , TPS61280 I check the datasheet. It seems there is no difference between theses 2 parts. Do I miss somthing ?? Is there any difference between TPS61282 and TPS61282D ??? also TPS61280…
Jasper,
I have a question not associated with the programming of tps61280, but with its bypass mode. Could it conduct current in the opposite direction in a bypass mode? For example to charge the battery, allowing current from the host side through the…