Part Number: TPS62000-HT Other Parts Discussed in Thread: TPS62000 ,
Hello,
I am using twoTPS62000 to power a SM470R1B1 with 1.8V and 3.3V.
At 187C the 3.3V starts fluctuating between 2.9V and 3.0V - this is critical because it resets the microcontroller…
Part Number: SM470R1B1M-HT Hello,
I am using the SM470R1B1M-HT in a high temperature system, powered by two TPS62000 DC/DC converters, one for 1.8V and one for 3.3V.
At 185C, the circuit has a jump in current from 20mA to 35mA. The voltage of the 3.3v…
Shawn / Alexander,
TPS62000 is rated for 150C Tj as highlighted in the datasheet. However TPS62000-HT is is rated up to 210C. On ATE tests on the TPS62000-HT device is subjected to the higher temperature per the datasheet parameters where as the external…
Chris,
I clear all other filters but High Temp, then only two products show up (TPS50301-HT and TPS62000-HT). There should be more.
Did I use the search engine incorrectly?
Best regards,
Wai-Ming
Part Number: TPS61222 Other Parts Discussed in Thread: TPS40210-HT , TPS62000 Hello all,
A customer is looking for a boost converter that can operate at 150C-200C.
He found TPS61222 but this only operates at 125C. Thus, he asked me that " Can I use…
Other Parts Discussed in Thread: TPS54362-HT , TPS62000-HT Hi Team, Is there any device that can operate under the following condition? -------------------------------------- ・Vin: 5.4V ・Vout: 2.6V ・output load: 0.35A(MAX) ・fsw: 3MHz ・Ta: 125℃ -----------------…
Other Parts Discussed in Thread: TPS62000 , TPS62000-HT
Hello,
We are currently evaluating a TPS62000 based 5V to 3.3V power supply especially used at very high temperature. On the evaluation board right now we use a TPS62000QDGSRQ1 device, which then…
Other Parts Discussed in Thread: TPS62000 , TPS62000-HT Hello,
Sorry for a double post, but I already posted this question into the DC/DC converter forum, but now I was not sure if this was the correct location, and therefore
I thought it is best to ask…
Hi Nikhil,
If you are developing a model for the TPS62000-HT please set it up so it can be simulated in the inverting configuration.
Is it possible for you to upgrade the TPS62110 model to allow the inverting configuration?
Thank you for your consideration…