Part Number: TPS62082 Hey,
I am designing a power management solution to generate 3.3V output with max. 1A. The Input will come either from an USB-Plug (5V, up to 2 A)or an LiPo with a range of 3V to 4.2V.
Is it possible with the TPS62082 to generate…
Part Number: TPS62082 Hello there,
I am using the step-down TPS61253YFFR with a fixed 3.3V output voltage. For the output capacitor C308 = 22uF I use GRM21BR60J226ME39L as provided in the data sheet.
Could you please give me a review regarding my schematics…
Part Number: HD3SS3220 Other Parts Discussed in Thread: TPS62082 , TPS62080 Hello!
I need help for schematic review.
My application will works in UFP mode. I have a little confused about Fig.12 in the HD3SS3220 datasheet and "UFP dongle evaluation module…
Hi Alfonso,
I scoped between pins 2 and 5 on the IC and still get 3.25V.
The oscilloscope and multimeter readings are the same and there are no fluctuations in the reading on the oscope.
The voltage input is 4V coming from a TI charger connected to a…
Part Number: TPS62082 Other Parts Discussed in Thread: LM3281 , TPS62821 , TPS62172 , TPS62561 , TPS62170 , TPS62230 , TPS62056 Hi,
I'm looking for LM3281 replacement that converts 5V to 3.3V. I cant solder BGA packages and LM3281 is BGA. QFN or any other…
Dear Emmanuel,
It has been a while since we were in contact.
In the meantime we found the reason for the erratic behavior of the TPS62082 on some of our boards.
It turned out that on the defective boards the coil L2 in series with the SW output was shorted…
Other Parts Discussed in Thread: TPS62081 , TPS62082 Dear all
I'd like to know which part does load regulation show on graph?
for example Io=10uA to 1.2A? or 200mA to 1.2A?
Other device is called PWM mode.
Could you please current point on spec condition…
Part Number: TPS61252 Other Parts Discussed in Thread: TPS62082 , , TPS61251 Hi TI Technical Support Team,
I have designed a board that has some low power sensors powered by TPS62082 IC (IMU, leds etc) and 2 motors and buzzer that are powered by 5V supply…
Other Parts Discussed in Thread: TPS62082 , TPS61251 Hi TI Technical Support Team,
I have designed a board which have some sensors (Temperature, humidity, accelerometer etc), buzzer and motor driver IC (TB6612) on it. The power to the board is from 1S 2200mAh…