Part Number: TPS62097-Q1 Hello TI team,
there is no available document for Pin FMA on the product page of TPS62097-Q1. I would like to inquire if you can provide additional information about Pin FMA for that part.
thanks & best regards,
Hanjie Li
Part Number: TPS62097 I'm having issues with a very small number of TPS62097PWKRs.
When raising a specific TPS62097 from Vin: 330mV to 3.3V, the following two problems will occur.
(It operates normally when Vin rises from just under 300mV.)
・Vout…
Part Number: TPS62097-Q1 Other Parts Discussed in Thread: TPS62097 Dear TI colleagues,
TPS62097-Q1 is supporting pri-bias SS. Nevertheless TPS62097-Q1 is having also discharge function with 165ohm in silicon.
This function will occur the problem that…
Part Number: TPS62097 We are using TPS62097 on several of our boards.
Does this device have any problems if it is started with voltage present on the output?
This is the case when output capacitors are not completely discharged and enable signal is applied…
Part Number: TPS62097 Hi team,
Could you explain the meaning of EN pin specification? see below table.
Why Vh_en min. value is 2V and typical value is 1.6V?
Why the definition is not like Vh_mo?
Currently customer GPIO voltage is 1.8V, so is it ok to…
Part Number: TPS62097 Hi TI,
I just noticed at no load, the SW will see spikes higher than maximum rating... Even the screenshot from EVM seems to show the same thing:
So this screenshot is taken from https://e2e.ti.com/support/power-management-group/power…
Part Number: TPS62097 Hi team,
What is the softstart time without Css? In datasheet, minimum softstart time can be achieved by removing Css but datasheet does not reveal what will be the value.
Part Number: TPS62097 I observed some ringing at the SW node, which causes it to have negative spikes at every switching cycle. I measured close to -2V for about 5ns. In the datasheet the minimum voltage specified is -0.3V for SW pin. Is this spike acceptable…
Part Number: TPS62097 Other Parts Discussed in Thread: TPS62093 Hi TI support,
Regarding the VIH_EN threshold for TPS62093, may I know what is the difference between 1.6V and 2.0V?
What is the risk if I connect my VIH_EN to
1) 1.6V?
2) 1.7V?