Part Number: TPS62130A Hi Sirs,
The TPS62130A design spec is
Vin: 3.3V;
Vout: 1.15V
I_load: 0.16A
Fsw: 1.25MHz
Could you help check the switch node at light loads (0.16A), is it operating in power save mode?
We measure the min switching…
Part Number: TPS62130A Please check following compare products website.
compare products
I think some features have been deleted or erroneous.
Would you please fill in the yellow highlighted cell in the attachment?
6825.comparison.xlsx
Regards…
Part Number: TPS62130A-Q1 Other Parts Discussed in Thread: TPS62130 We are using 2 TPS62130 in a low voltage regulator in order to drive an ir source (1.3V) and for 5V board power
All components are aligned with power designer except additional filtering…
Part Number: TPS62130A Is there any significant leakage into the TPS62130A when VIn is powered down (0V) and voltage (say 3.3V) is applied to the PG pin?
Part Number: TPS62130A We've done several products with the TPS62130A, with acceptable EMI performance. We have followed the TI recommendations for laying out the components around the part.
The current product is showing excessive EMI, possibly due…
Part Number: TPS62130A-Q1 Dear team,
This device is used to power the USB. When the customer hot plug the USB several times, our device has no output. At the same time, VIN and EN is normal. I am not sure whether our device is damaged. Could you please…
Part Number: TPS62130A We use TPS62130A on our custom board and now I am testing. Used of condition is below. Vin = +5V, Vout = 3.3V and +2.5V (Number of TPS62130A on the board is two.) We measured voltage of Vout and Vin with oscilloscope in the power…
Part Number: TPS62130A Other Parts Discussed in Thread: TPS62130 , What is the PG pin used for and what are the differences between the TPS62130 and TPS62130A?
Part Number: TPS62130A Dear E2E Design Support,
I have been using the TPS62130A in several designs, but recently I encountered a radiated emission issue with a new board which made me thinking about the right layout topology, especially how to connect…
Part Number: TPS62130A Other Parts Discussed in Thread: TLV62150 Dear Specialists, Customers need FMEA information to adopt new parts. Please tell me the FMEA information of TPS62130A and TLV62150. It helps in design-in.
Best regards, Yusuke