Part Number: TPS62130A-Q1 Other Parts Discussed in Thread: TPS62130 We have estimated the power dissipation on the TPS62130A-Q1 mounted on a 10-layer HDI PCB as 0.7W based on measured data.
The thermal resistance parameters mentioned in the datasheet…
Part Number: TPS62130A-Q1 I setting the switching frequency as 2.5MHz.
but why in my measurement the maximum switching frquency only 1.56MHz.
for variable switching frequency, how can I calculate the indutance?
my condition:
Vin=8V, Vout=1.09V, Iout…
Part Number: TPS62130A-Q1 Other Parts Discussed in Thread: TPS62903-Q1 , Hello TI Team,
We are using TPS62130AQRGTRQ1 in our design and having following observations:
1. We are having an application of converting the 5V input to 3.3V output. The inductor…
Part Number: TPS62130A-Q1 Hello,
I was asked to perform bode tests on a board with the component listed above. I was wondering if DCS devices such as this can even obtain valid network analyzer results. The plots I have taken appear valid, but I wanted…
Part Number: TPS62130A-Q1 Hi Team,
Good day. I am posting this inquiry on behalf of the customer.
"I encountered a problem with my 2.5V DC converter (see U5). The input is 5V with an output of 2.5V. Currently, the prototype is not output 2.5V but rather…
Part Number: TPS62130A-Q1 Hi, Expert:
I found TPS62130A-Q1 datasheet Figure-50 1.8V 3A application FB pin R1 /R2 resistor were 360K/160K , the Vout=2.6V not 1.8V with VFB=0.8V in the datasheet page 28. Figure 50.
can you check the figure have something…
Part Number: TPS62130A-Q1 Hello Support,
I have seen the reference design of TPS62130AQRGTRQ1 and want to convert 12V to 5V,3A output.
Since it is a buck convertor what minimum input current is required with 12V input voltage?
Since it is not linear regulator…
Part Number: TPS62130A-Q1 Since the test of Rjctop and Rja of TPS62130A-Q1 are unrelated, I still need the value of junction-to-case thermal resistance(Rjc) instead of junction-to-case(top) thermal resistance for 2R thermal evaluation. I was wondering…
Part Number: TPS62130A-Q1 Other Parts Discussed in Thread: TPS62130A Hello team,
I received a question from my customer about the specifications of the TPS62130AQ1.
Because TPS62130ARGTR they previously used became difficult to obtain, they are considering…
Part Number: TPS62130A-Q1 Other Parts Discussed in Thread: TPS62130 We are using 2 TPS62130 in a low voltage regulator in order to drive an ir source (1.3V) and for 5V board power
All components are aligned with power designer except additional filtering…