Part Number: TPS62133 Other Parts Discussed in Thread: TPS62130 , Hi
I am using TPS62130 to generate a 5V voltage in a mass production product. I want to know is there any risk if I directly replace TPS62130 with TPS62133, don't remove the feedback resister…
Part Number: TPS62133 Other Parts Discussed in Thread: TPS62130A-Q1 , TPS62140 , TPS62140A , TPS62150 , TPS62130 , TPS62130A , TPS62150A Could you please let me know when this part will become available? Or could you suggest an alternate part that is available…
Part Number: TPS62133 Other Parts Discussed in Thread: DRV8870 , On our PCB we plan to use the TPS61233 to generate a stable 5V (1A load) and motor driver DRV8870 (max. 2A load) sharing the same 12V input. Is there a risk that load changes on the DRV8870…
Part Number: TPS62133 Hi,
Can TPS62133 (5V fixed output) provide a regulated output when the input voltage is 5V? What would be the approximate output voltage considering the drop across mosfet and inductor?
Part Number: TPS62133
Hello,
I am using the TPS62133 for a 5V / 2.5A supply. 5V_PSU.pdf
With no load, I measure 5V, howerver with approximately 250 mA, the voltage rail drops down to 4.6 V.
It keeps dropping down with higher current demand.
Is there any…
Part Number: TPS62133 At this moment we have designed a PCB for a customer where we use 3x TPS62133A for generating 3 different +5V supplies out of +12V. For the input we use a 10uF/25V/X7R/1206 cap in parallel with 100nF and at the output a 22uF/10V…
Hi Aaron_Rangel , Please be informed that non automotive version i.e. TPS62133 is also updated and is functional on production. Feel free to contact us for any further queries. Thank you
Best Regards, Sateesh A G
Hi Ian,
The TPS62133 and almost all DC/DCs (even most battery chargers) have current limit protection. So, the IC will protect itself by limiting its output current. You can read the D/S for an explanation of how the current limit works in this device…
Part Number: TPS62143 Other Parts Discussed in Thread: TPS62133 , Dear team,
I wish to know whether the TPS621433RGTT is fully replaceable with the TPS62133RGTT (pinout and layout means).
Best Regards,
Itay
Hi,
I have a very similar problem in my project with TPS62133: it fail without apparent motives.
Could you try to post the images with the micro crack?
Best Regards,
Fabio