Part Number: TPS62150A-Q1
Our customer is considering to use TPS62150A-Q1.
They have a question about dynamic current limit.
There is following description in datasheet P11.
-----------------------
The current limit can exceed static values, especially…
Part Number: TPS62130 Other Parts Discussed in Thread: TPS62150A-Q1 , Customer is currently using 2 devices for 2 output rails:
TPS62130RGTR deliver 1.5V @ 500mA
TPS62150AQRGTTQ1 deliver 3.3V @ 450mA
Due to shortage, they want to qualifying either device…
Part Number: TPS62130A Please check following compare products website.
compare products
I think some features have been deleted or erroneous.
Would you please fill in the yellow highlighted cell in the attachment?
6825.comparison.xlsx
Regards,
Part Number: TPS62150A-Q1 Hi, Good day. I hope you are well. Our customer wants to use the TPS62150A-Q1 on their design and they want to protect the 5V VDD output for short circuit to Battery and GND. So, they have added a general purpose diode between…
Part Number: TPS62150A Other Parts Discussed in Thread: TPS62150
When the TPS62150 input voltage is lowered to about 6.5V, its IQ will suddenly increase to 9mA, compared with a normal IQ of about ten uA. Is this normal? How to solve it?
Part Number: TPS62150A-Q1 Hi team,
My customer asked question about UVLO.
Q.1) In Table.2, it describes "0.7 V < VIN < VUVLO". Does "0.7V" meand 0.7xVin, or simply 0.7V?
Q.2) Customer want to toggle PG when Vin goes down to 6V…
Part Number: TPS62150A Hi team,
My customer is evaluating TPS62150A. Could you support the following question?
The customer would like to use a total resistance of 500ohm (R1+R2) for the FB resistors. Is that acceptable?
Regards,
Yamaguchi
Part Number: TPS62150A Tool/software: WEBENCH® Design Tools Hello team,
my customer wants to use the TPS62150A due to the good efficiency with light loads and at 1.25MHz. On Webench they ran a simulation and the inductor chosen of 2.2uH is screened and…
Part Number: TPS62150A Other Parts Discussed in Thread: TINA-TI , Tool/software: TINA-TI or Spice Models I have a customer who received the unencrypted model for the TPS62150A and is having issues with the model.
The customer stated that when he clicked…