Part Number: TPS62152-Q1 Hello,
I would like a sanity check on my design. I bought thru hole components to prototype the buck converter but I underestimated just how small the QFN 16 package is, and unfortunately the tools at my disposal have made it…
Part Number: TPS62152 Hello Experts, I have question about absolute maximum ratings of SW terminal. My customer is evaluating TPS62152 and measured SW terminal voltage during light load condition. Please see attached link. He saw high overshoot and undershoot…
Part Number: TPS62152 Hi,
Kindly let me know the time(Off time) from enable to output when enable is low(Output also low) of TPS62152RGTR
Warm regards,
Monisha OM
Part Number: TPS62152 Hi! We designed a home IoT alarm system and for the External warning device we are using the TPS62152 buck regulator as a power supply. Our input voltage is 12V(8x AA battery in series). We are trying to verify the power supply efficiency…
Part Number: TPS62152-Q1 Other Parts Discussed in Thread: TPS62152 , TPS62150 Hi
Greetings, I'm considering to use TPS62152 or TPS62152-Q1 discharge function on the VOUT, but the description in the datasheet confuses me.
Could you kindly help me to…
Part Number: TPS62152 Other Parts Discussed in Thread: TPS62147 Hello,
I was wondering what happens, when the output sees a voltage with the input floating or grounded? Would that go beyond the abs max of Vin+0.3? So maxmimum would be 0.3 V at the output…
Part Number: TPS62152-Q1 Other Parts Discussed in Thread: LM1086 Dear TI,
The circuit is composed as shown below.
The test result shows that the output voltage is 3.15V. The output I want is 3.3V.
What's wrong with the output? Does the output voltage…
Part Number: TPS62152 When i import it into eagle it shows hole cutouts and i don't know how to fix it.
This is what it show in eagle
This is what it shows inUlitra libaran