Part Number: TPS62175EVM-098 Hello,
My customers are evaluating using this EVM.
Could you provide DC bias characteristic data of C1, C2,? Or please tell us the model number of the capacitor.
Thank you.
Other Parts Discussed in Thread: TPS62175EVM-098 , TPS62175 , TPS62172 , TPS62150A Hello
I am evaluating the TPS62175EVM-098, which should have a 3.3V fixed output voltage with 500mA max. current. The input voltage was 12-13.8V.
Using a 10 Ohm load the output…
Hi Kim,
Thank you for sharing your schematic and layout.
The layouts are pretty bad and do not follow the D/S example in Figure 62. Especially since you have plenty of PCB space around the ICs, it is much better to keep all components on the same layer…
This is shown in the package drawings at the end of the D/S: pages 34 and 35.
A picture of one is found on the EVM: http://www.ti.com/tool/tps62175evm-098 There will be a mark/dot/line in the quadrant noted by the package drawing.