Part Number: TPS62810-Q1 Hi team,
I have question about the 100% duty. If the input voltage is 5V and we want to ouput around 5V @ 1.5A, is there feasibility? I guess, it should be in the 100% duty mode and the output voltage should be 4.91V (Ron(60mohm…
Part Number: TPS62810-Q1 Hi TI Flores,
I looked at the datasheet and found that the TOS6381x series has built-in descharge function and I'd like to ask how this function helps POL? (Except time sequence)
Is it to prevent the Mosfet from being burned…
Part Number: TPS62810-Q1 Other Parts Discussed in Thread: TPS62810 Can the level of the TPS62810 EN exceed the VIN? Currently VIN=3V3; EN=5V, if it is possible to cause a current drain
Part Number: TPS62810-Q1 Due to supply shortages, I am considering which parts to choose to fulfill a 300pcs trial board build. My original design uses automotive-grade, but for this new build I can use standard-grade in order to move forward.
My question…
Part Number: TPS62810-Q1 In the datasheet, Figure 10-58. "Schematic for Output Voltage Tracking", an application circuit is provided for tracking a second supply voltage from a main supply voltage using the SS/TR pin and resistive voltage divider…
Part Number: TPS62810-Q1 I'd like to set a custom UVLO voltage for my +5.1VDC input (DC/DC generates a +3.3V output). What resistor value range is suggested, 10Ks...100Ks...Megs? And, are there any equations I should use (accounting for hysteresis…
Part Number: TPS62810-Q1 Hi, Support Team
Our client use TPS6281020-Q1, Please help to review schematic as below chart
if any suggestion, Please advise me.
Thanks,
Best regards,
Lawrence
Part Number: TPS62810-Q1
Dear team,
Our TPS62810-Q1 only has one package, but there are two package outlines in the datasheet, RWY0009A and RWY0009C. The difference between these two outlines is as below. Then for TPS6281120QWRWYRQ1, which package outline…
Part Number: TPS62810-Q1 Hi team,
Customer is considering change from TPS62810QWRWYRQ1 to TPS6281020QWRWYRQ1 due to supply consideration. Just would like to confirm TPS6281020 spread spectrum is default enabled and cannot be disabled? Customer worries…
Part Number: TPS62810-Q1 Hi Expert,
Our customer is looking for TPS6281120QWRWYRQ1 replacement due to shortage. They mainly focus on the same series, such as TPS6281220QWRWYRQ1 ; TPS6281320QWRWYRQ1 ; TPS6281020QWRWYRQ1. They have difference output current…