Part Number: TPS63020 Hi, I made the typical application with Vout=3.3V. The load drain from 30 to 140mA dynamically and powered with stable voltage 3.18V provide by lab power source. Some times the regulator fail, Vout go to ~1.4V, working alone. One…
Part Number: TPS63020 Other Parts Discussed in Thread: TPS631011 , TPS61033
Tool/software:
Hi TI team, We are planning to implement a o utput discharge function using Power Good pin for the TPS63020.* Could you indicate what is the maximum current…
Part Number: TPS63020-Q1 Tool/software: Hi,
I'm using the TPS63020-Q1 as a 3.3V buck boost converter for a lithium-ion battery with an input range of 2.6V to 4.1V. This powers a BLE module which, depending on the transmission level spikes between 30…
Part Number: TPS63020 Other Parts Discussed in Thread: PMP9759 Hello,
I am using the Pspice model for the TPS63020 and configuring it to drive a TEC (simply modeled as a 2 Ohm resistor). I am making connections as shown in the app note, PMP9759. The…
Part Number: TPS63020 Hi team,
Customer get one question when 5Vin and 5Vout operation. Does TPS63020 get bypass mode? In customer case, does it work in bypass mode?
Thanks and Best regards,
Will
Part Number: TPS63020 Hi:
I made the schematic of a typical application (Figure 7 on datasheet) but no placed R3; Vout=3.3V.
Without any load drain 5.38mA from power source, but doesn't must be equal to Iq 25~50uA?
Thanks!
Part Number: TPS63020 Other Parts Discussed in Thread: TPS63802
Hi.
I want to be able to supply a board with 3.3V or 5V, and regulate to 3.8V~4V to supply a 2G/4G module. When the module operates in 2G/GSM/GPRS mode, it can draw peaks of up to 2A…
Part Number: TPS63020 Hi,
I heard that TPS63020 is a bidirectional DC-DC converter, the output energy can go to input. can you tell me in which condition this can happen?
Thanks,
Tony
Part Number: TPS63020 Other Parts Discussed in Thread: PMP9759 When using the TPS63020 as a TEC driver, and configured per the app note PMP9759, does the power supply that is feeding the TPS63020 input need to be able to sink current? When the TEC is…