Part Number: TPS63050 Hi team,
My customer received an notice of the TPS63050 datasheet has been revised recently,
they are using the TPS63050YFFR with DSBGA package, and would like to ask a following 2 questions,
1. what's the change of the pin configurations…
Part Number: TPS63050 Hello, I've got a design on which I'm trying to stabilize the voltage on a very sensitive (to ripple) module. The module would normally receive 5.17V and the ripple is constrained at max 35mVpp. Occasionally the input drops…
Part Number: TPS63050 Hi, Good day. I hope you are doing fine. Our customer is using the TPS63050RMWR and they have question about its soft-start. 1. Does the Vout ramp quicker if SS pin is left floating (no capacitor connected) OR if a 1nF capacitor is…
Part Number: TPS63050 Other Parts Discussed in Thread: TINA-TI , , TPS62801
Hello there.
I have spent quite some time in trying to stabilize the outputs of switching regulators provided by TI. I would like to specify two devices here, the TPS63050 and…
Part Number: TPS63050 Other Parts Discussed in Thread: TPS63060 , TPS63070 Hi,
Planning on using the TPS63050/1. Some batteries types will have MAX 5,8V, is this harmful for the IC when the spec is 5,5V max but absolute max is 7V?
Thanks
Part Number: TPS63050 Hi Team,
I would like to quick check of TPS63050's input current limit(inrush current limit) setting, as d/s ,
IIN_MAX at the spec Vin=2.7V to 4.5, Vout-4.5V , ILIM0=HI,ILIM1=HI the max input inrush current is 1950mA(max),
…
Part Number: TPS63050
Hi there,
My customer would like to check if it is fine with 2.2uH and 22uF. Vin is 3.3V and output is 3.85V/24mA. The 22uF is a 6.3V ceramic.
Thanks.
Part Number: TPS63050 Hi, I have a TPS63050RMWR in my design and it seems to do the job. But I've got a couple of boards here in front of me that were working at one point, but not are not working, and I've traced the root cause to an unexpected voltage…
Part Number: TPS63050 Hello,
I am having issue with using the TPS63050 spice model (unencrypted). When I simulate a circuit using the TPS63050 spice model in Altium 17.1
I get an error
Class Document Source Message Time Date No.
[Error] TPS63050 XSpice Error…