Part Number: TPS650250 Other Parts Discussed in Thread: TPS62441-Q1 , TPS6521905 , TPS6593-Q1 Tool/software:
Application detail:
We are looking for a Power Management Integrated Circuit (PMIC) that can provide 3.3V, 1.8V, and 0.9V outputs. This PMIC…
Part Number: TPS650250-Q1 Other Parts Discussed in Thread: TPS650250 , Hei Team,
What ESD rating of TPS650250QRHBRQ1?
Although we checked datasheet and we confirmed with TI Customer support center,we could not find any information.
Best regards…
Part Number: TPS650250-Q1 Other Parts Discussed in Thread: TPS650250 Hi team,
I could found Power-up sequencing in this datasheet. the sequence is controlled by EN pins for each DCDCs. However, I couldn't find power good pins.
would you please advice…
TPS650250 has an Operating Temperature Range of -40°C to +85°C , and a maximum Junction Temperature (TJ) of +125°C
TPS650250-Q1 has an Operating Temperature Range of -40°C to +125°C , and a maximum Junction Temperature (TJ) of +125°C
The difference…
Yada-san,
You have two options:
Set TPS65023-Q1 LDO output voltage to 2.8V = 101b or 3.0V = 110b and test to see if either of these will work for your 2.8V requirement. 3.0V will produce 2.9V if you ensure the I*R losses in the trace from LDOx output…
Hi Yimin,
TPS650250-Q1 can not support J5Entry low power mode (standby, sleep), as it has no I2C interface, see below e2e thread:
e2e.ti.com/.../488603
TPS659119-Q1 has I2C interface and also many other features comparing with TPS650250-Q1,…
Hello Uma,
I can't find any single PMIC which has the same number of rails, and is externally configurable. Usually with that many rails, we use OTP-configurable devices.
We do have smaller devices that could be put together in the system to meet…
Other Parts Discussed in Thread: AM3358 , TPS650250-Q1 Hello,
We have found a problem when trying to boot a custom board based on AM3358. The following steps have been performed:
Booting from the UART0: 1 Connect the AM3358 UART0 to a PC 2 We receive…
Hello Komatsuda-san,
Looking at your requirements, I would suggest either of the following
TPS650250 :
VIN: 2.5-6 V
3 Buck converters, 3 LDOs
All externally adjustable with resistor dividers
Separate enable pins for sequencing
TPS65053…