Part Number: TPS65100 Hi,
I wanted to quickly verify that equation 8 in the datasheet on page 21 ( https://www.ti.com/lit/ds/symlink/tps65100.pdf#page=21 ) doesn't have a typo. Should the equation have " 2 *π*C8*R1" in the denominator as opposed…
Part Number: TPS65100-Q1 Team,
can you please advise what is the recommendation on FB4 and Gate pins if the LDO is unused ? on the non Q1 version we can see that FB4 and gate should be connected to VIN.
thanks
Part Number: TPS65100 Hi Apps,
I am a TI focus account DFA in the Americas.
We have a customer in my territory that is doing a high volume embedded design using an LCD & with our TPS65100.
They have a previous locked support question here:
https:…
Part Number: TPS65100 Other Parts Discussed in Thread: TPS61500
Hi Team,
Please help review TPS61500 schematics, thanks!
PB_SCH_EVT_V01_20230509_TI.pdf
Part Number: TPS65100 We have been using the TPS65100 on numerous design with great success.
We have a design that has been n production for over a year.
Recently, the LCD manufacturer revised the module, which resulted in the need to reconfigure the…
Part Number: TPS65100 Other Parts Discussed in Thread: TPS65101 I needed to replace a TPS65101 on a prototype by a TPS65100. The TPS65100 was originally intended to be used, however due to bad availability we had the TPS65101 assembled instead.
The outputs…
Part Number: TPS65100
Hello, I have some problems with the TPS65100. My display has these requirements:
AVDD: 10,2V @ 25 mA max.
VGH: 20V @ 1 mA max.
VGL: -10V @ 2,5 mA max.
VCOM: 4.3V @
Initially after a few seconds it went into fault mode, and I understood…
Part Number: TPS65100 Hello,
My name is Thai.
Can you help review this schematic please.
Right now, I can only achieve Vo1 (9.5V).
Vo2 is giving me 1.1V and Vo3 is giving me 0V.
I'm trying to achieve VGH = 20V and VGL = -6.8V
Thank you very much…
Part Number: TPS65100 Dear Sir,
We are using TPS65100 for Powering LCD where we need AVDD=10.4V, 400mA, VGH = 16V, 4mA, VGL = -7V, 4mA, and VCOM = 3.6V. We are facing some problems with the below-attached schematic, Some time start and build all power supplies…