Part Number: TPS65296 Good afternoon,
I have an issue with switching node of VDD1 and VDD2 when the load is light.
'TPS65296: Vmin of switch exceeded during light load', I already see this created issue but I couldn't see the solution proposal.
…
Part Number: TPS65296 Hi all,
There is TPS65296 as a power supply to LPDDR4. Is there any product other than TPS65296 that supplies power to LPDDR4? I hope to configure multiple power products and input to LPDDR4. Please tell me the recommended product…
Part Number: TPS65296
Hello,
We noticed that the package drawing information of TPS65296 doesn't match the real component footprint.
Is Texas Instruments aware of this issue or I just receive a counterfeit part?
Best regards,
Marco
Part Number: TPS65296 Hi Sir,
After power on, the shell temperature of TPS65296 rises above to 85 ℃ quickly (Ambient temperature 25 ℃ ). Then the power chip triggers the thermal protection mechanism.
What are the possible reasons for this…
Part Number: TPS65296 Hi,
TPS65296 has two VDD: VDD1 and VDD2, since my customer only request VDD2 for power supply. we would like to know how to deal with VDD1?
1)CAN we float PIN-SW_VDD1?
2)Can we connect PIN-VDD1SNS to 1.8v since we prefer to…
Part Number: TPS65296 Hi,
I will be using a Xilinx MPSOC devices with a 32 bit-4Gb LPDDR4 device. Max bandwidth MPSOC can go is 2400Mbps.
So basically I wont need 8A or 1.5A from both outputs of TPS65296 and I will be dependent on power calculators…
Part Number: TPS65296 Dear sir,
Please help to check if the schematics design is ok or not, thanks!
PVIN = 12V
PVIN_VDD1 = 5V
Load: Micron LPDDR4 4GByte * 2pcs
This PMIC is design for the power supply of LPDDR4 , so we don't need the LDO channel…