Part Number: TPS6594EVM Hello , i have three questions ,
I am using the TPS6594EVM to connect to an external PMIC in a a custom board , the PMIC adress is 0x28 , is that normal?
When i try to program the PMIC i get this error , i connected the I2C…
Part Number: TPS6594EVM Hello ,
I am having issue flashing the NVM into the TPS6594x EVK .
It was working just fine before , i want to make sure that the NVM is lot premanently locked.
how can i Check the contenet of the register 0x41 in page 1…
Part Number: TPS6594EVM Other Parts Discussed in Thread: TPS6594-Q1 Hi TI Support Team,
I am currently working on a power design using the TPS6594-Q1 PMIC and am in the process of configuring the PFSM (Pre-Configurable Mission States) via the Scalable…
Part Number: TPS6594EVM Hello TI support team,
I have a new TPS6594EVM board that I cannot program due to what appears to be security locks in the PMIC, here's my situation :
Board: New TPS6594EVM (TPS65941212EVM)
Connection: SPI via Scalable…
Part Number: TPS6594EVM Tool/software: SCH_of_PMIC.pdf
Dears
Two power boards were designed using TPS659411 to supply power to the DSP core, BUCK1+BUCK2+BUCK3+BUCK4. Board A uses a 12 layer PCB design with capacitors placed on the bottom layer, while…
Part Number: TPS6594EVM Tool/software: it shows HW connected, but no devices detected
I used default I2C settings, but it does not connect, so I switch to SPI mode on GUI without changing jumper on EVM, connected, but no devices detected.
Can…
Part Number: TPS6594EVM Other Parts Discussed in Thread: TPS6594-Q1 Tool/software: Hi,
there are 3 questions.
1. Is there any detailed information about SPMI? In the datasheet, there is no description except for GPIO
2. Does the board support SPMI…
Part Number: TPS6594EVM hi,
1: I notice my TPS6954 1212 EVM has 5 Phase configurations, could you tell me what is "1212" Phase config?
I search it "1111" is Phase config 1, "1213" is Phase config 2. Please see my picture.
if we choose wrong config…
Part Number: TPS6594EVM Hi, all:
I want to turn on and turn off TPS6594 LDO, BUCK output in the different time. because my design has requirement for power up and down sequence.
1: when PMIC is working, all LDO and BUCK output normally, if I am using…