Part Number: TPS65986EVM Other Parts Discussed in Thread: TPS65981EVM
I am trying to configure the TPS65986EVM to power and enumerate USB3 devices. I'm using the default firmware.
The test device is a Samsung USB Flash drive. When plugged directly…
Part Number: TPS65986EVM Hi,
Now I am review the TPS65986 schematic.
And I found the L11 and B6 pin which is define to NC pin, but it still connect to GND and K10 pin on our TPS65986EVM schematic.
Do those pin should just keep unconnected or I should…
Part Number: TPD4E05U06 Hi,
My customer has the following question:
I have question about the TPD4E05U06 surge suppression device. In the datasheet, pins 6, 7, 9, and 10 are either not connected, optional straight thru routing or floating or grounded…
Part Number: TPS65986EVM Other Parts Discussed in Thread: TPS65982 Hi
Could you help to provide TPS65986 EVM CAD files with PCB and SCH?
I have one customer "DKVE" request it. pls help
BRs
Eric Lo
Part Number: TPS65982-EVM Other Parts Discussed in Thread: TPS65986EVM , TPS65981EVM , TPS65981 , TPS65982 I need to make a system for a vehicle, electric skateboard, but those are my first steps with USB Type C
I need charger the battery pack of the skate…
Part Number: TUSB1046EVM Other Parts Discussed in Thread: TPS65982 , HD3SS460
Hi~
I want to test with the TUSB1046EVM.
I want to control the TPS65982 PD chip that is configured on the TUSB1046EVM board.
If I look at the TPS6598x configuration tool, it…
Part Number: TPS65986EVM Hi,
Looking at the schematic for the TPS65986EVM, RPD_G2 is connected to the L11_NC net. Is this necessary for some reason/ should we put this in?
Thanks,
Josh
Part Number: TPS65986EVM Other Parts Discussed in Thread: DP-EXPANSION-EVM My customer is having difficulty getting DP1.1 to work over our TPS65986EVM and DP-Expansion-EVM. They have verified that the video source is good and that the display (Dell U2410…
Part Number: TPS65986EVM Other Parts Discussed in Thread: TPS25740A I'm designing a USB type-C device for a customer that connects to an Android phone. The solution needs to charge the phone as well as appear to the phone as a USB 2.0 device (USB-serial…
Part Number: TPS65986EVM Other Parts Discussed in Thread: DP-EXPANSION-EVM , HD3SS460 I have been unable to get USB 3.1g1 data flow using the TPS65986EVM with the DP-EXPANSION-EVM in the client configuration. In fact, in most cases, I can't even get a USB…