Part Number: TPS65987EVM Hi,
I have a problem with TPS65987EVM
In adapter-> settings, the following message appears:
Exception Encountered during I2C Address Sweep:*** ERROR in FTDI call (I2C_OpenChannel), status: 3
<type 'exceptions.Exception'>…
Part Number: TPS6598X-CONFIG Other Parts Discussed in Thread: TPS65987D I am getting the "SPI Flash to Device failed verification" error pop-up after attempting to "Flash from current project" onto the TPS65987EVM.
Here are my flash…
Hi Rutvik,
When using your project (TPS65987_Field_Demo3.pjt) with the TPS65987EVM (as the sink) and TI's USB-C-PD-DUO-EVM (as the source) and selecting a 5V contract, so the <15W (PDO 0), the D22 glows for me as seen in the picture below:
I am…
Part Number: TPS65987EVM
I'm attempting to set up my TPS65987EVM to function as a 5V, 3A sink with DisplayPort Alternate Mode (UFP_D) and USB 2.0 data transfer over USB Type-C. Despite creating a customized project file, my laptop fails to detect an external…
Part Number: TPS65987EVM Hi Technocrats, I have a tps65987EVM and to configure that I need to I installed tps6598x customization tool, on windows 11 from the given link https://www.ti.com/licreg/docs/swlicresults.tsp?countryName=India&eeq=Civil&Certify…
Hi Field,
Awesome, u are a star. Thanks for your advice regarding EEPROM, To write the configuration in EPROM am I supposed to program the PD controller SPI pins or Configuration is going to be stored in EEPROM automatically? Looking at the Config setting…
Hi Klaus,
The reason the PD is rebooting upon barrel jack removal is because VIN_3V3 is removed before the barrel jack event can be detected on the GPIO. Once VIN_3V3 is removed and the PD is in normal operation mode (non dead battery), the PD will shut…
Part Number: TPS65987EVM Hello - we have used the TPS65987EVM board to make a working product prototype. We now have designed a board with the TPS65987 and we need to program it in production over SPI. Can you recommend a suitable programmer that will…
Part Number: TPS65987EVM Hi,
Can you please share the schematic design files for the TPS65987EVM in Altium format? I see only the layout design files. I understand there are PDF schematics, but it would be very helpful to have the design files to speed…