Part Number: TPS65987EVM Hi, I'd like to download the SOURCE configuration file for EVM DUO source board. I tried "Device > Re-Flash EVM Firmware Recovery" When I select the SOURCE configuration binary it fails with an exception saying that it ha a NULL…
Part Number: TPS65987EVM Hello:
In the UCC28782EVM document, they mention PM110.
It cannot be found anywhere.
We are not yet ready to fork out $1000 bucks for testing with anything other than Electronic load, maybe HPIB.
A real question is : does the…
Part Number: TPS65987EVM
Why is the output 22V when I select 20 V output?
I see the schematic also indicates that 22 v will be output for the 20V configuration.
What is the thinking behind this?
Part Number: TPS65987EVM Hi,
We are designing a Dock that can deliver 100W PD source (20V, 5A max) in DFP mode and has USB3.2 HUB for downstream ports.
We have the below queries:
1. For our application TPS65987D looks suitable. We checked the TPS6589…
Part Number: TPS65987EVM Hello I read thru the posts on the failures of the TPS65987EVM and do not see the resolution on this Testing.
We are about to plan and proceed with purchase: pl advise the safe approach, At the end of this testing, we would like…
Part Number: TPS65987EVM The actual board is an TPS65987-90EVM. I have tried several drivers, and two different Windows 10 systems, as well as restarting both systems, and trying various power up/connection procedures.
There is no indication on Device…
Part Number: TPS65987EVM OK.. Here are the Spec sheets for the Connector on the EVM. But I can't find the raw Plug end anywhere
Does anyone have any leads?
DC-PowerJack-JPD1135-509-7F-FOXCONN-JPD1135-509-7F.pdf JPD1135-509-7F.pdf
Part Number: TPS65987EVM Hi,
I am trying to flash the board from recovery image from the folder "C:\Program Files\Texas Instruments\TPS65981_2_6_7_8 Application Customization 6.1.3\tps6598x-application-customization\recovery"
Image name "tps65987_power_duo_mode_SINK_evm_flash_image…
Part Number: TPS65987EVM When running the TPS6598x Application Customization Tool (version 6.1.1 or version 6.1.3), in debug mode and under the Debug Register tab, there are two registers called; Received Battery Status Data Objects (BSDO) Register (0x7a…
Part Number: TPS65987EVM HI We want to test the EVM. In this as per gui reference videos we want to flash the binary code with the help of GUI code to set the current and voltage as per our application. i got the gui but did not got any binary code.
…