Part Number: TPS6598X-CONFIG Other Parts Discussed in Thread: TPS65987D ,
Hi Team, My customer designs their application with TPS65987D. Regarding TPS6598X-CONFIG, they made the project (.pjt) from Version 6.1.1 previously however current version of GUI…
Part Number: TPS65987EVM I am trying to configure a TPS65987EVM for D_DFP_D using the Application Customization Tool. I have entered Debug mode and am looking at the Configuration Registers. Every time I change the Port Capability from "DP_UFP_D and DFP_F…
Part Number: TPS65987EVM Hi team,
I'd like to use TPS65987DDH EVM as sink and I use GUI default example.
When I enter the debug mode, I cannot see the Transmit Sink Capability(0x33), and I also check the power path status, the PP1 switch (sink) is…
Part Number: TPS65987EVM Dear TI,
I flashed binary file to EVM DUO source board and tool show successfully, but it seem it is not working. I don't see led VBUS and any led source 5V, 9V, 15V or 20V light although i pressed S1 to S4.
How we can check…
Part Number: TPS65987EVM Hello,
I'm attempting to use the TPS65987EVM to supply 20V to a custom PCB that uses a TPS65981 for USB power delivery. I'm using the TPS65987EVM for USB-C Alternate Mode DisplayPort as well as 20V/3A power delivery, but…
Part Number: TPS65987D Hello, We're attempting to test a TPS65987DDH chip on a custom PCB and having a bit of trouble getting an established USB contract going. We're using a TPS65987EVM as the DFP port to test power delivery. The custom PCB has sink…
Part Number: TPS65987EVM Hello Team,
I am struggling to update Region pointer oFFSET address in SPI Flash attached onboard with TPS65987EVM
I am preparing a program to flash SPI as it is our requirement in fresh production board where we are going to…
Part Number: TPS65987EVM Good Morning,
Could You send me design files for USB-C-PD-DUO-EVM and TPS65987EVM.
I saw only PCB design files but not schematic files in editable format.
Best Regards,
Jake.
Part Number: TPS65987EVM Hi Team,
I would like to set configuration of TPS65987EVM by “TPS659xx Application Customization Tool”.
The setting method is as follows but I can't change VBUS of DFP.
(Even if I set it to 9V(PDOs is 2), it will…