Hi Eric,
v6.1.4 is the current version of TPS6598x GUI.
Eric Koch said: Can you flash my binary ( tps_bug.zip ) I attached two week ago and do a raw register feed as well?
Using the tps_bug.pjt these are the raw register read results using debug mode in…
Part Number: TPS65988 Other Parts Discussed in Thread: TPS65987 , TPS25751 Hello TI -
Our client is wondering what can be done from within the constructs of the TPS65988 - it's internal registers or it's interrupt events (which may or may not be enabled…
Part Number: TPS65988
Hi,
I have a custom board using TPS65988 and TUSB1046 that converts a DP connection from the source PC to a USB-C output DP-ALT compatible sink. From my PC as the source, I have the board hooked up to a DP sink analyzer and I can…
Part Number: TPS65988 Hello,
we need to supply device in powerbank mode with TPS65988CERJTR.
The minimum power required is 30W.
could it possible to negotiate 5V 6A contract ?
Regards,
Elvina A.
Part Number: TPS65988 Other Parts Discussed in Thread: TPS65981 Hi
I'm designing a PCB using TPS65988DHRSHR PD-CTRL for USB-C Charging Ports. During Bring Up I have encountered two problems:
1. The TPS65988DHRSHR is connected to an external flash memory…
Part Number: TPS65988
Hi Team,
I'm testing TPS65988EVM with FTDI on board and I follow up user guide below:
https://www.ti.com/lit/ug/slvub62b/slvub62b.pdf?ts=1712592950328&ref_url=https%253A%252F%252Fwww.google.com%252F
Switch S3 is default…
I tried using the "New contract as provider" IRQ. When using the PD logger, I see that the source accepts the request, but the interrupt is triggered only when using the 5V PDO, for other PDOs, I see the request is accepted but the IRQ is not triggered…
Part Number: TPS65988 Hi,
I have been working on a new board bring-up. This is the 7th revision of the board. All previous revisions of the board work as expected, but on this revision something unexpected occurred with the TPS65988 bring-up.
We have a…
Part Number: TPS65988 What is the difference between TPS65988DHRSHR and TPS65988DJRSHR?
For TBT3 device can see that Intel use TPS65988DHRSHR in their reference design Tapex Creek TI88
For TPS65988DHRSHR and TPS65988DJRSHR,Which one is currently recommended…