Hi Aya,
From the schematics I provided, which can be downloaded from the link https://drive.google.com/file/d/1f2K5-UazeKBZn4N49QNV16L_pLlBCZNt/view?usp=sharing , you can see that the USBC (CN1) VBUS is only connected to PD, without any other components…
Part Number: TPS65988DJ I want to use TPS65988DJ to implement the PPS function of PD3.0
, I want to ask where can i find the TRM (Technical Reference Manua) of TPS65988DJ. I want to use TRM to understand how to modify the data in the register to realize…
Part Number: TPS65988DJ Other Parts Discussed in Thread: TPS65987
Hello .
I'm designing the Thunderbolt titan bridge Tapex Creek TI88.
The guide says to use the TPS65988DJ.
Is there any problem using TPS65988DH?
If there is a problem, can the problem…
Part Number: TPS65988DJ Other Parts Discussed in Thread: USB-C-PD-DUO-EVM status:
We have used TPS65988DJ to manage 2 ports USB-C output, the power capacity is 5V/3A and 15V/3A. (no TBT circuit)
Application Customization Tool (6.1.4) has no configuration…
Part Number: TPS65988DJ Hello everyone,
can someone tell me if it's normal to obtain these waveform on CC signals when we use this IC on.
Because, nromally, we should have either 0V or 3.3V depending on the orientation of the cable !
one more question…
Part Number: TPS65988DJ Other Parts Discussed in Thread: TPS65982DMC , TPS65988DK Hi
Would you please review TBT4 GORILLA TI design (TPS65988DJ+TPS65982DMC)?
Please add me friend let me send schematic via privacy message. thanks!
Jeff
Part Number: TPS65988DJ Hi sir,
My customer is starting a tapex creek TBT3 dongle project and modify it to bus power application. We can load code into 988 and finish alt mode communication. And we can see first IRQ clear process (didn't get Logic analyzer…
Part Number: TPS65988DJ Hi,
Would you please help for layput review?
I will pass schematic and layout file via privacy massage, please add me friend. thanks!
Jeff