Part Number: TPS65988EVM Hello
Can I get the schematics and PCB design files for the TPS65988EVM ? That would help me a lot.
Thanks a lot,
Regards
Eric
Part Number: TPS65988 Hi All,
Is TPS65988EVM EOL? Please tell me the reason for EOL. Also, are there any EVMs that can replace TPS65988EVM?
Best Regards, Ishiwata
Part Number: TPS65988 Hi,
I'd like to use TPS65988EVM to implement two typec port feature simultaneously.
Port 1 works on UFP on the sink side, only sink power from a PD charger, no need for high speed signal.
Port 2 works on DFP on the source side…
Part Number: TPS65988DKEVM Other Parts Discussed in Thread: TPS65988DK Hello there,
Can I receive the config file(EEPROM data) on the FTDI debug board of the TPS65988EVM?
Thanks,
Sam
Part Number: TPS65988EVM Hi there
Could you send me TPS65988EVM layout file?
It would be helpful for me to understand TPS65988 better.
Thanks
Br. Chulwoo
Part Number: TPS65988EVM Hi team
I would like to demo TPS65988 to customer, I want to configure the EVM as monitor port which can work as power source and video sink, how can I configure the EVM.
thank you!
Hi Chris,
Thank you for confirming for USB2!
I have been prototyping to use TPS65988EVM to source 20V over the external PP_EXT (PP3) path when the sink requests 20V. At all other voltages (5V, 9V, 15V), I would like to use the internal PP_HV1 switch instead…
Part Number: TPS65988EVM Hi,
I'm trying to control TPS55289 from TPS65988 via I2C. I followed the instructions in "Using I2C Master in TPS65987D and TPS65988 PD Controllers" ( www.ti.com/.../slvae18.pdf
Current setup:
TPS65988EVM: default…
I have ordered a new TPS65988EVM for delivery tomorrow morning. Would you suggest I continue with the TIVA interface or leave the board with the FTDI interface?
Thank you very much,
Roy