Part Number: TPS727 Hi Team, Do we have a TI part with almost 0 minimum load current to offer with our customer? His minimum load should be in the range of 1ua to 5uAs. Our datasheet shows 0 mA load current but upon testing for TPS727, its minimum is around…
Part Number: TPS727 Other Parts Discussed in Thread: TPS7A20 Hi,
I am using the TPS72733 to regulate an input voltage of nominal 3.7V. All works fine but when the input voltage falls to around 3.3V (the regulation voltage) the current consumption of the…
Part Number: TPS727 Other Parts Discussed in Thread: LP5907 Hi Team,
I'm looking for a replacement for the ADP121 - must be ok with Vout greater than Vin conditions, drop out compatible with a 3.3V supply load current about 10mA, and PSRR 70dB or better…
Part Number: TPS727 We noticed that the "pin A1" marking on P/N TPS72730YFF (DSBGA, 4 pins) is above the A2 ball rather than above the A1 ball (per the data sheet). Can you please confirm that this is indeed correct (e.g., that the mark is over…
Part Number: TPS72715DSEEVM-406 Other Parts Discussed in Thread: TPS727 I am trying to use Tina to look at the fast transient resposne for a number of TPS parts. In particualar the TPS72715 set to 4.6 or 5 Vout. What are the parameter settings needed for…
Part Number: ADS1262 Other Parts Discussed in Thread: LM27762 , TPS727 , TPS61099 , ADS1261 Can you advise on the ideal power components for a 5v reference on the ADS1262 with a single 3.6v battery? Specifically for running a loadcell.
There are a ton of…
Rick,
Have a look at TPS706 and TPS782 in the SOT23 package. Those are good alternatives.
If you need a chipscale option, TPS727 comes closest to meeting those requirements.
~ Aaron
Hi Avatar,
Please take a look at the TLV733P, TPS720, and TPS727 families. Each of these families include a 1.5V fixed output option in a small package size you list.
Very Respectfully,
Ryan
Other Parts Discussed in Thread: TPS727 Hello LDO team,
Have you measured the output impedance of TPS72730 vs frequency? If so, could you please provide a graph?
Many thanks, Esa
Other Parts Discussed in Thread: TPS727 Dear Sir
May we have TLV70048 part? Due to from DS,
Available in Fixed-Output Voltages from 1.2 V to 4.8 V. but we can't find 4.8V parts.
Best regards,
Bo…