Part Number: TPS730
We usually use an external drop-out diode protection to protect the LDO during programing or when the output is higher than the input. The reverse current has not been specified in the datasheet. Could you please let me know what…
Part Number: TPS730 Hi Team,
May I ask if +/-2% accuracy in TPS730 is over full temperature range(-40~125C)? If not, then what's the accuracy over full temperature?
I suppose it should be, as it's written in the datasheet that only typical values…
Part Number: TPS730 Hi Experts,
a customer approached me since they have some concerns with changing their BOM from a TPS73018DBVT G4 to TPS73018DBVT. In the past there used to be differences between those part numbers, but according to the product homepage…
Part Number: TPS730 Other Parts Discussed in Thread: TPS737 , TPS745 Hi Team,
May I know the difference between TPS7370 and TPS74501?
Are they P2P replaceable?
Thanks and best regards,
Jamie
Part Number: TPS730 Hi,
The block dig arm of TPS730 has one 59K pull down at the output. is it for discharging the output voltage when LDO is disabled?
Can I test this resistor value as per below procedure.
1. Put LDO to shutdown more (EN=0)
2. Force…
Part Number: TPS730 HI,
I have one more query regarding the Feed back pin current testing.In TPS730 datasheet the specification is below.
For testing this, Need to force 1.8V from ATE to FB pin and check the current ?
What should be the status of output…
Part Number: TPS730
Hi,
we use TPS73001 for 5V to 2.5V/100mA convertion, C_NR=10nF, feedback resistor R_top=33K, R_bottom=32K, Cff=18pF. As SCH picture below.
TPS73001 claims fast start up time about 50us, and I guess the actual ramping time is enven…
Part Number: TPS730 Hi
My customer evaluate TPS73033.
However the inrush current is over 200mA.
Are there the provision about inrush current?
Best regards,
Yokota