Part Number: TPS732 Hi
I am using TPS73201DCQR LDO.Input voltage is 3.3V and output voltage is 1.8V/200mA.When Resistor load.is connected It is observed that output drops below up to 1.72V and output ripple is arround 348mV peak-peak.
Test snap of…
Part Number: TPS732 Hi team,
My customer is evaluating TPS73250, he noticed that fig.10 current limit vs. vout was tested with TPS73233, can we provide a similar figure for TPS73250?
Or should we consider that the same as TPS73233, -0.2V~0.5V will be…
Part Number: TPS732-Q1 Other Parts Discussed in Thread: TPS732 Dear team,
DCQ package information and thermal metrics are nowhere to be found in the datasheet of TPS73218QDCQRQ1.
Can you share with me these details ?
Thanks a lot!
Best regards,
PA
Part Number: TPS732 Hi Team,
I wanna know more about the parameters in the data sheet.
When the output current is 10mA, is it quiescent state?
As I know about quiescent current, it is the current drawn when the device is enabled and there is no load…
Part Number: TPS732 Hi team,
Do we have suitable LDO for P2P to replace adjustable output version of LDO of SGM2036-ADJ? and the price is as low as possible.It is used in the Thermostat of household air conditioner.
At present, I choose TPS73201. Can…
Part Number: TPS732 Hi!
I have an application where the TPS73225DBVR is fed with very instable input voltages, which could cause the LDO to be switched on and off successively with T<20ms. Vin and EN are tied together.
The first time the input voltage…
Part Number: TPS732-Q1 Other Parts Discussed in Thread: TPS732TPS73250QDCQRQ1 has DCQ package. The part's datasheet does not seem to contain pinout diagram for this DCQ package. Where do I get the information?
Datasheet is www.ti.com/.../tps732-q1 …
Part Number: TPS73233-EP Other Parts Discussed in Thread: TL431 , TPS732 Can we cross check the temperature drift of this IC by using a voltage reference taken from TL431 IC?
The latter only tells, it's a low temperature drift IC but doesn't give a value…