Part Number: TPS734 Hello,
The part I'm using is the TPS73401DDC. Page 8 of the TPS734 datasheet in the Feedback Capacitor Requirements section (on the middle right hand side) says:
The feedback capacitor, CFB, shown in Figure 21 is
required for…
Part Number: TPS734 Other Parts Discussed in Thread: TPS784-Q1 , TPS784 Hey team,
I had a customer that was looking at these two parts and doing a brief comparison of the two. They highlighted the difference in startup time specified between the two datasheets…
Part Number: TPS734 Hi team,
My customer designs this device and the package will be DDC.
But there is no board layout and Stencil Design figure in the datasheet, so could you provide them to me?
Or send complete datasheet to me as well?
I need to forward…
Part Number: TPS734 Other Parts Discussed in Thread: TLV62130A Hi,
Please could you share any construction details of the shielded 5100uF AC-coupling cap (Figure 3 in white paper "How to measure LDO noise", SLYY076)? I'm interested in both the…
Part Number: TPS734 Other Parts Discussed in Thread: LP5900 , Some regulators spec output noise as a proportion of Vout, such as noise (uVrms) = 11 x Vout. Other datasheets specify noise as an absolute number such as noise = 11 uVrms. Are the differences…
Part Number: TPS734 Other Parts Discussed in Thread: TPS732 , I would like to know if the TPS73401 can use the soft start circuit as in SLVA156 figure 6 (app note says there are certain regulators that this circuit will NOT work with)?
My second question…
Hi Chris,
The ADS122C04 datasheet does discuss other implementations including 4-wire RTD in section 9.2.2.2.1 and demonstrated in figure 76 using a low-side reference. More combinations and details regarding various connection scenarios are in the A Basic…
Hi Ian,
Thanks for sending this over. Here are a few devices that may fit your requirements: TPS734, TPS735,LP2989, or TPS799.
If you are open to using adjustable-output LDOs then I'd really like to recommend the TPS7A90 which actually has a 10uF capacitor…
Other Parts Discussed in Thread: TPS734 Hi team,
Do we have clamping diodes in front of the TPS73401 on the EN pin TPS73401 ? If yes, how much current do the clamping diodes (protection diodes) support?
Thanks in advance.
Pol
Hi Waqar,
For Vout of 0.8V to 5V+:
The TPS7A83/4/5 and TPS7A87/8/9 family of devices are targeted at low-noise, high PSRR rails for Iout = 500mA to 4A.
Other parts to look are the TPS717 (150 mA), TPS734/735 (250mA/500mA), and the LP5907/10/12 (250…