Part Number: TPS735-Q1 I am conducting the FMEDA for an ECU that uses TPS73515QDRBRQ1. Please may I have the component fit rate as per SN 29500 and the FMD aswell.
Thank you,
Bushra
Part Number: TPS735-Q1 Hi team,
My customer is carrying out FMEDA activity on one project and the manufacture number is TPS73512QDRBRQ1.
But I couldn ’ t find any functional safety information( failure rate, failure mode, failure distribution and others…
Part Number: TPS735 Hi,
I have a customer using TPS73501DRB, and he wants to know whether the soft start time of this chip is adjustable, if so, how much capacitance is needed to adjust to at least 100us, is there a reference formula?
Many thanks~
Part Number: TPS735 Hi,
Due to the customer's circuit design, the input voltage becomes 0 V⇔ about 1.5 V before the TPS735 starts.
At this time, is the voltage output from the OUT pin (1 pin)?
When I look at the internal circuit, EN(5 pin) and…
Part Number: TPS735 Hi
I have a question about TPS73501DRVR EN turn on VS VOUT and EN turn off VS VOUT, from figure 18 shown in datasheet, the turn on time is about 50us, but there is no figure about turn off time, in my circuit the COUT=22uF, can you…
Part Number: TPS735 Hello team,
Customer question translated with TI-Translator,
Today, a tricky question. I am using the TPS73501. I set the VOUT voltage with a DAC. The signal is called "IR_DAC". "IR_DAC" is generated with an 12bit DAC, max. 3.0V output…
Part Number: TPS735 The Vin and EN are connected together, the power on sequence is as follows.
the yellow waveform is Vout, blue waveform is Vin, why does Vout follow Vin when the EN pin is less than the threshold voltage? I think that Vout should be…
Part Number: TPS735-Q1 Other Parts Discussed in Thread: TPS735 Hi team,
The package of TPA735 and TPS735-Q1 are a little difference.
The customer want to use TPS735 replace TPS735-Q1 without changing PCB. Is that ok?
thanks. : )
regards,
Cathy
Part Number: TPS735 We recently bought stocks from online distributors for an NPI project and noticed difference in lead frame between COO Thailand and COO China. are both valid lead frames and will it affect the application?
Thanks in advance!
COO …