Part Number: TPS73701DRVEVM-529 Hi
When we try to simulate TPS73701 in LTSPICE, we get error "Too few nodes ....", and I download spice model from TI own website.
When I search why that error arise from, I understand that Spıce Model which…
Part Number: TPS73701DRVEVM-529 Hi
When we try to simulate TPS73701 in LTSPICE, we get error "Too few nodes ....", and I download spice model from TI own website.
When I search why that error arise from, I understand that Spıce Model which…
Part Number: TPS73701DRVEVM-529 Other Parts Discussed in Thread: TPS737 Hi ,
We are planning to use TPS73701DCQ LDO in our design .
We have the below query .
We are using LTC2977IUP for Servoing . Is the TPS73701DCQ Feedback node voltage okay to…
Part Number: TPS73701DRVEVM-529 Hi
I have a question about TPS73701 current limit.
When I was testing TPS73701 OCP, the output current retried as red below.
Is this normal behavior?
Ch1: Vin
Ch2: Vout
Ch3: En
Ch4: Iout
schematic:
Thanks
BR,
Hank
Part Number: TPS73701DRVEVM-529 Hi Team,
We are using TPS73701 Adjustable LDO in a battery powered design. When the device is in deep sleep mode, we observed that the voltage divider network is consuming more than 100uA of current with the resistor divider…
Muhammed Junaidh M said:
Part Number: TPS73701DRVEVM-529
Hi All,
I am using TPS73701 LDO regulator in my design. In my design, I have a 2.8V input power supply for this regulator with an expected output current load of 100mA. My output voltage is 2.7V…
Part Number: TPS73701DRVEVM-529 Other Parts Discussed in Thread: TPS737 Hi ,
Our spec is Vin=5V, Vout=4.75V, Imax=0.4A.
Can TPS73701 meet its spec?
If not, do you have another suggestion?
Part Number: TPS737
Hi all Would you mind if we ask TPS737? <Question1> Do you have VFB(Internal reference) data with Tj=-40 to 125C? The data sheet shows in case of Tj=25C. So, there is the description "Over operating temperature range (TJ = –40°C to 125…