Part Number: AWRL6432 Other Parts Discussed in Thread: TPS746-Q1 , TPS745-Q1 Hi team,
I have a question here that since my customer would like to use LDO to provide the power for 1.8V and 1.2V. I recommended they use TPS745-Q1 and TPS746-Q1 which has…
Part Number: TPS76833-EP Other Parts Discussed in Thread: DRV8301 , TPS54160 , TPS768 , TPS746 , TPS746-Q1 Hello TI, I wish you a happy new year!
I have a motor controller board that has a few issues with quite a noise (80-100kHz) on the 3.3V rail…
Part Number: LP38502-ADJ Other Parts Discussed in Thread: TPS746 , TPS7A91 , TPS7A83A , TPS7A90 Hi team,
My customer is looking for a LDO to supply a sensor. The constant current is 485ma, the peak current is 980ma. The input voltage is 3.3v, the output…
Hi,
At 1.2V OUT , the TLV757 has an effective R DSON of 1.1-Ohm:
So at 800mA, the worst case drop would be 880mV which means that the TLV757 could not do this. However, the TPS746 can.
I hope this answers your question.
Hi Inho Jeon,
For VR1 - NCP4687DSN25T1G - I would like to recommend TLV755P - specifically TLV75525PDBVR as a P2P option.
For U75 - ADP1752ACPZ-1.0-R7 - I would like to recommend our TPS746 or TPS7A80 devices.
regards,
Wilson
Thank you Stephen...incase 1.8V is typical input ...apart from below listed..will you recommend with high PSRR and Low noise.
TPS785-Q1
TPS784-Q1
TPS745-Q1
TPS746-Q1
TPS76201-Q1
Regards,
Harish
Hi Saito-san,
Currently, we do not have an active project to release a fixed 0.95V option of the TLV757P. Please contact me with the customer details so we can see about kicking this off.
The alternatives you suggest are good ones, we also have…
Hey Diverger,
Unfortunately, we do not have any P2P alternatives to this device.
TPS7A92 is a lower noise option that does not require a bias supply. TPS746 is a smaller solution that still has a PG output signal.
I hope this helps!
Thanks,
…