Hi Srijesh,
It looks like for the 3.8V output, TL1963A-Q1 might be an option. Its quiescent current with a 0mA load is 1.5mA max, though, which is higher than your requested 500µA max.
For the 3.3V supply, I'd suggest TPS74801-Q1 or TPS748A-Q1 as…
Part Number: TPS75333-EP Other Parts Discussed in Thread: TPS74801 , TPS753 , TPS7A8300 , TPS748A We have used TPS75333QPWP in a previous application and are looking at using it in a new application. However, the RESET timeout delay of 100ms is a little…
Hello Kei,
The Bias and quiescent may be referred to the same current in a bipolar LDO, but in modern LDOs they are different.
In modern LDO's, the bias current is inherent of NMOS LDOs as they do require a higher voltage bias rail to power their…
Hi Ernest,
We have devices that have an internal soft start, and we have other devices that use an external pin to adjust the soft start timing.
Based on the information provided, you are looking for a device that allows to control the soft start…