Part Number: TPS761 Hi team,
My customer considers to use TPS76132DBVR and TPS76032DBVR because of other IC supplier's EOL.
Is it okay to apply voltage on NC pin as much as input voltage for these devices?
Best regards,
Shota Mago
Part Number: TPS761 Is there p2p compatible with TPS76150 since customer is looking for higher voltage up to 20Vin?
Condition:
Input Voltage: +15V, 5% accuracy
Output Voltage: 5V
Output Current: <20mA
Application: Current Module
Hi John,
Unfortunately we do not have a model for this device as the original commercial version was released ~20 years ago so a model wasn't created. Can you use one of the models released for the TPS761 to do your simulation? This part has very similar…