Part Number: TPS769 Hello,
I have a query on the TPS76950 5V output SOT23-5 Linear regulator. I'm using it at low output current 1 - 2mA and would like to know the approximate typical output voltage tolerance over -20 degree C to +55 degree C. If this…
Part Number: TPS769 Hi E2E,
Good day!
We just need some clarification regarding the minimum required input voltage for this part. On page 3, note 2 states that Vin mimum is equal to Vo + Vdo. Vdo values are indicated on page 5. However, on page 4, Note…
Part Number: TPS769 Other Parts Discussed in Thread: TPS767 , Hi all I am using TPS76950 Fixed 5V regulator in my system which has following powerparameters
Input Voltage: 6V
Output voltage: 5V
Peak current consumption: 70mA
Constant current current consumption…
Part Number: TPS769 Team,
My customer likes the TPS76950, however he has concerns on the requirement of 0.2 to 10 Ohm ESR for the output capacitor:
I do not use tantalums unless there is no other way. An aluminum electrolytic can meet this 10SVPS10M .…
Hello Coeleen,
The table below compares the specs of the devices. It is the same die size but have different fab sites as well as different compound specs. I will confirm if there is a specific reason why TPS76901HDBVT was EOL without LTM, but sometimes…
Part Number: TPS784-Q1 Other Parts Discussed in Thread: UA78L , TPS7B69 , TPS7B81 , TPS709 , TPS769 Hi Team,
There is a good new that we could DIN TI product!
Customer is looking for the replacement of SGM2203-5.0YK3G/TR
Please help suggest TI solution, T…
Other Parts Discussed in Thread: TPS769 , DRV2603 Hi Team,
I'm looking for the vibrator driver IC solution replacement part for MAX1749,
we are used this part for touch screen application ,when people touch the screen , it will trigger the vibrator…
Hello Andy,
It looks to me like the MAX1749 is a linear regulator IC. I cannot locate a direct drop in replacement due to the unique pinout of the MAX1749, however the TPS769 is a capable replacement. The MAX1749 requires an output capacitor with ESR…