Part Number: TPS7A02 Part TPS7A02 is not in PSpice for TI 23.1-2024 S001 How to add it manually from the zip archive downloaded from Ti.com? The zip file does not contain .olb file. A hack is to use the part cached in Design Cache of the example schematic…
Part Number: TPS7A02 Hello,
I would like to ask you a question about TPS7A02. I'm currently checking the behavior of EN and output voltage. The waveform is shown below. In the waveform, OUT was output when the EN voltage was 0.8V. VEN(HI) in the datasheet…
Part Number: TPS7A02 Hello,
I would like to ask you a question about TPS7A02. (Question) Do you have MIN and MAX data regarding Ren (pulldown) in the electrical characteristics below? I am currently checking whether the startup time is affected by the value…
Part Number: TPS7A02 Dear team,
1. DoesTPS7A02 series has minimum current requirement? my customer find when leave Vout float, the output of TPS7A0215PDQNR becomes around 1.6V. I see in recommend ratings we have 0-200mA output range
(they use a very weak…
Part Number: TPS7A02 Hi,
I am using TPS7A0230PDBVR, the datasheet note with capacitor output "22 µF is the maximum derated capacitance that can be used for stability".
What happen when i use 100uF.
Thanks,
Part Number: TPS7A02 Hi TI Teams,
Can u help to confrim that did TPS7A02 support 1.3V input and 1.2V output? If yes, how much conversion efficiency can be achieved at this time?
Thanks,
Kind Regards
Part Number: TPS7A02 Hello Sir
Customer is using a battery source to power TPS7A0233, and they want to disable the TPS7A0233 when battery voltage is 3.5V.
We want to know, how to design a user defined input under voltage lockout function by using EN pin…
Part Number: TPS7A02 Hi team
If you have the date of Dropout Voltage with Iout=20mA, please send us the date. If you don't have it, please support this request.
Thanks
Iza
Part Number: TPS7A02 Dear Sirs,
My customer product is Tag related product and they found they can't use TI LDO with the smart enable function.
Without smart enable function will no problem.
As their design, they will use tag at the first power on…