Part Number: TPS7A33 Hello.
I'm trying to interpret Figure 28 of the datasheet which seems to show a positive output when the regulator is in the disabled state. I am assuming that the central grid line is 0V. Is this the effect of some external circuitry…
Part Number: TPS7A33 Other Parts Discussed in Thread: TPS63710 Hi,
Below is my schematic arround TPS7A3301RGWT for my custom board, i have tried to maximum follow the EVK
But still i wish to know if there are any flaws in my layout
Kindly have a look and…
Part Number: TPS7A33 Dears:
Customer happen to connect 24V to TPS7A3301 Vout, then IC was damaged. Could you please help advise how to add protection in this PIN? Or Do we have other LDO can support this application? Thanks.
Part Number: TPS7A33 Hello, could you recommend an alternative product for the TPS7A3301RGWR, which is pin compatible and has the same package.
Thanks and regards.
Juan Camilo Peña A.
Part Number: TPS7A33 Hi,
I am using TPS7A33 to generate -15 V from -16.5 V. The issue I met is the chip would fail consistently after a long term working. The output shows 0.65 V after the failure happen. In the data sheet, I found that the chip could…
Part Number: TPS7A33 Hello,
Will you please confirm part marking PPQQ is TPS7A3301KC?
The TI part marking lookup tool doesn't include PPQQ in the database.
Thank you,
Part Number: TPS7A33 Hello,
I have several questions for Table 2, Suggrestiged Resistors For Common Voltage Rails, in the datasheet(SBVS169D) of TPS7A33.
When R1 = 0 ohm and R2 = Open case, the table says that VOUT = -1.171V. But NOM VREF value should…
Part Number: TPS7A33 Hello,
My customer is desiging TPS7A33 circuit and need the maximum voltage on NR/SS pin to select the capacitor for this pin. Could you tell me it?
Regards, Oba
Part Number: TPS7A33 Other Parts Discussed in Thread: TPS7A47 I am working on a design which uses TPS7A3301 for generating -2.5V output using an input which can go till -6V. One of the requirements I have is to drive the output pin externally using an…
Part Number: TPS7A33 Hello,
My application requires having a -9.7V which is capable of sourcing current up-to 400mA. I wanted to ask if TPS7A33 has current sourcing capability. Its datasheet mentions that it is capable of providing 0 to 1A of current…