Part Number: TPS7A3301EVM-061 My company also needs mechanical info on this eval board. We are including it in a very early prototype we have to ship.
Basically we mainly need the diameters and separation of the two holes for stand-offs. This could come…
Part Number: TPS7A3301EVM-061 How does this device get mounted. There appear to me two mounting holes,. What are their dia. and location from the edges?
Thanks,
Part Number: TPS7A3301EVM-061 I designed a 4 channel +/-3.3vdc power supply board using tps7a3301 and tps7a8300. Each channel has 750mA loads. There are 4 tps7a3301 ic for each channel and 2 tps7a8300 ic sharing between 2 channels. The board has 4 layers…
Part Number: TPS7A3301EVM-061 Tool/software: TINA-TI or Spice Models Please provide me with the unencrypted spice model for the above Vreg.
Thanks,
Uttara
Hello I have a problem with the TPS7A3301EVM-061.
In practice, I would benefit from going out to-12V.
From the datasheet of the regulator TPS7A3301 the values of the resistors R1 and R2 are, respectively,-12V Recommended for: R1 = 1.5 Mohm R2 = 162…
Hi Kenji,
You should be okay using tantalum or OS capacitors with these LDOs; however, as with any application design change we recommend prototyping before making the change. This way you can see how the change impacts your system before making the change…