Part Number: TPS7A47-Q1 Hi team,
When I add the input from 5V to 20V and the output is kept at 3.3V, is it normal for the device temperature to go from 30 degrees to nearly 100 degrees?
If the maximum input voltage of the device of 35V needs to be reached…
Part Number: TPS7A47-Q1 Other Parts Discussed in Thread: TPS7A47 Hi team,
I have some questions about LDO front-end capacitor selection. As mentioned in the user manual, the input voltage range of TPS7A47 is -0.4~36V, in Typical Application chapter, the…
Part Number: TPS7A47-Q1 Other Parts Discussed in Thread: TPS7A47 Hi,
When TPS7A47's output is short when VIN=36V, VOUT=1.4V and IOUT is short. Therefore the power dissipation on pass FET will be about 36*1.26=45W. Will thermal shutdown protects the device…
Part Number: TPS7A47-Q1
Hi Team,
My customer is using TPS7A47-Q1 and recently reports 5 failure cases (in total 30 boards).
Background:
1) Input voltage: 24.5~28V (Input comes from the multi-windings Flyback, it's the aux-winding output and varies due…
Part Number: TPS7A47-Q1 Hi Team,
My customer use TPS7A47-Q1 in his automotive project.
He use it in a 10Vin / 9Vout 500mA Max. load design.
Now he had a output keep short to GND test, need to make sure our device safety include the thermal perform.
He…
Part Number: TPS7A47-Q1 Hi team,
My customer would design TPS7A4701QRGWTQ1 in his project.
Do we have the TPS7A4701QRGWTQ1 Maximum & Minimum value of VREF can provide to customer?
Thanks!
Kai
Part Number: TPS7A47-Q1
I am using the voltage regulator for 3.3V output. Below is the circuit I am using.Issue I am facing is that whenever I give Vin =25V from battery source.The regulator gets burnt.Due to this my MCU gets damaged aslo.Please suggest…
We don't have anything more modern in that metal can, but here is a link to a filtered version of our parametric search which shows the positive voltage linear regulators that we do have in a metal can.
If you wanted to assess newer options I'd start…
Part Number: TPS7A47-Q1 Other Parts Discussed in Thread: TPS7A47 Hi team,
May I have your help to propose the LDO solution automotive solution to meet below requirements?
Vin = 10.5V
Vout = 10V
Iout = 1A
AEC-Q100 is needed
Is TPS7A47-Q1 the best solution…